DOUT#.SOURCEID

Description

DOUT#.SOURCEID sets the digital output source ID, for sources that require an ID.

Examples

Usage

DOUT#.SOURCEID can be used to select the compare channel when DOUT#.SOURCE = 4 (Compare).

Code

The following commands set the source of digital output 2 to compare channel 1, and digital output 3 to compare channel 2.

--> DOUT2.SOURCE 4
--> DOUT2.SOURCEID 1
--> DOUT3.SOURCE 4
--> DOUT3.SOURCEID 2

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added Compare channel support 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 0
Data Type Integer
See Also N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen 0x360A DOUT1.SOURCE 0x1 USINT - - RW False
DOUT2.SOURCE 0x1 USINT - - RW False
DOUT3.SOURCE 0x1 USINT - - RW False
DOUT4.SOURCE 0x1 USINT - - RW False
DOUT5.SOURCE 0x1 USINT - - RW False
DOUT6.SOURCE 0x1 USINT - - RW False
DOUT7.SOURCE 0x1 USINT - - RW False
DOUT8.SOURCE 0x1 USINT - - RW False
DOUT9.SOURCE 0x1 USINT - - RW False